Comparing PCA Data
This option allows the user to compare two different dataset's PCA models with each other.
-
Click on the Compare Data button.
-
Data source selection:
-
Select the project data to use from All data, Brushed data or Non-brushed data. Note that only brushing that was performed before creating the model will be taken into consideration when using the Brushed or Non-brushed options. Once the PCA model has been created, you may brush in any of the trends without affecting the model.
-
Select a different dataset to be used for comparison from the populated drop down list. These datasets are those imported or created during Data Preparation in Step 1.
-
Apply limits: This will imposed the outer limits defined in the histograms on the new dataset fields for the PCA model comparison.
-
[Select] the dataset, then continue with mapping the new source’s inputs to those of the first data source’s PCA inputs. Click [Ok] when done.
-
-
Configure fields: define what to use as the batch index.
-
The two PCA models are then shown in the graph, the original in red and the comparison model in blue.
Note: Compared data will be lost once the view is closed.
Clearing the comparison data
To remove the comparison data click on the Clear Comparison Data button.
Related topics: